This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-DSP-EVM: MMWAVE-DSP-EVM Boot Issues

Part Number: MMWCAS-DSP-EVM

This is using the same DSP board that was identified as faulty in this post: New tab (ti.com). As TI and Mouser are no longer carrying this board I'm trying to find if there is a way to use the board and thought perhaps using a different boot method may circumvent the issue from the other post. I have several questions related to alternate boot methods.

1) I may have missed directions on how to use the other boot methods available on the DSP board, is there documentation you can provide from the USB, eMMC, & UART boot methods?

2) I couldn't connect to the board from MMWave Studio with the DIP switch on the DSP board set to eMMC (111000). Is there setup that needs to happen for the board to boot from eMMC, or is this indicative of an error?

3) The attached text file is taken from the start of the boot sequence of the DSP board. After the last line in the file (starting kernal) the system has a few failure messages and I can add those in a comment if requested, but for the most part the system reports normal booting. Are the errors in the attachment normal give I am booting using the SD card or is this due to an error?

U-Boot SPL 2016.05-00018-g6bc25a5 (Aug 05 2019 - 14:43:03)
DRA752-GP ES2.0
no pinctrl for hs200_1_8v
no pinctrl for ddr_1_8v
Card did not respond to voltage select!
*** Warning - MMC init failed, using default environment

Trying to boot from MMC1
reading dra7-ipu2-fw.lzop
spl_load_file_fat: error reading file dra7-ipu2-fw.lzop, err - -1
spl: error reading image dra7-ipu2-fw.lzop, err - -1
Error loading remotecore IPU2!,Continuing with boot ...
reading dra7-dsp1-fw.lzop
spl_load_file_fat: error reading file dra7-dsp1-fw.lzop, err - -1
spl: error reading image dra7-dsp1-fw.lzop, err - -1
Error loading remotecore DSP1!,Continuing with boot ...
reading dra7-dsp2-fw.lzop
spl_load_file_fat: error reading file dra7-dsp2-fw.lzop, err - -1
spl: error reading image dra7-dsp2-fw.lzop, err - -1
Error loading remotecore DSP2!,Continuing with boot ...
reading dra7-ipu1-fw.lzop
spl_load_file_fat: error reading file dra7-ipu1-fw.lzop, err - -1
spl: error reading image dra7-ipu1-fw.lzop, err - -1
Error loading remotecore IPU1!,Continuing with boot ...
spl: falcon_args_file not set in environment, falling back to default
reading single-stage-boot.dtb
spl_load_image_fat_os: error reading image single-stage-boot.dtb, err - -1
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img


U-Boot 2016.05-00018-g6bc25a5 (Aug 05 2019 - 14:43:03 +0530)

CPU  : DRA752-GP ES2.0
Model: TI DRA742
Board: DRA74x Cascade EVM REV H.4
DRAM:  4 GiB
MMC:   i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
OMAP SD/MMC: 0, OMAP SD/MMC: 1
Card did not respond to voltage select!
*** Warning - MMC init failed, using default environment

Card did not respond to voltage select!
ERROR: invalid mmc device

at arch/arm/cpu/armv7/omap-common/utils.c:193/mmc_get_part_size()
Warning: fastboot.userdata_size: unable to calc
SCSI:  SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net:   Could not get PHY for ethernet@48484000: addr 2

Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot:  0
## Error: "board_findfdt" not defined
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
switch to partitions #0, OK
mmc0 is current device
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
185 bytes read in 2 ms (89.8 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
switch to partitions #0, OK
mmc0 is current device
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
SD/MMC found on device 0
3577032 bytes read in 171 ms (19.9 MiB/s)
107792 bytes read in 24 ms (4.3 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x3694c8 ]
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Loading Device Tree to 8ffe2000, end 8ffff50f ... OK

Starting kernel ...