This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: AWR1843 to Raspberry Pi Connection

Part Number: AWR1843

Hello,

Need some help understanding the SPI code you have provided for connecting the AWR1843 with a raspberry pi?

Regards,

Adil

  • Hi,

    In order to use the SPI driver we recommend you review the unit test examples provided in

    C:\ti\mmwave_sdk_03_06_00_00-LTS\packages\ti\drivers\spi\test.

    The SPI code is provided "as is" with no support from our team

    thank you

    Cesar

  • Hello,

    I have another question, how and from where do I get the JTAG debugger? I am trying to use it to connect the Raspberry pi to the AWR1843

    Regards,

    Adil

  • Hi,

    I am not sure I understand this question.

    The AWR1843BOOST EVM has an XDS110 that is integrated on the EVM. This debugger can be used to access the AWR1843 ARM and DSP cores

    thank you

    Cesar

  • Thanks for the clarification Cesar!

  • Request for Information on mmWave SDK and SPI Master/Slave Code for the AWR1843BOOST

    Dear Cesar,

    I am writing to request some additional information and guidance on working with the mmWave SDK and specifically, the SPI Master/Slave code that is available. I have been working on a project that involves connecting the AWR1843BOOST radar sensor board to a Raspberry Pi 4 using SPI communication.

    I understand that TI has provided a modified version of the mmWave SDK demo that uses SPI instead of UART to communicate with the host. I am hoping to get some guidance on how to get started with this modified demo and how to modify the code to work with my specific setup. For example, where do I run it ? What program can I use to run the code ? Is it the code composer ? Do I run the master code on the raspberry Pi ? If so do I have to get the code composer on the Pi ? 

    Additionally, I would greatly appreciate any information you can provide on the SPI slave and master code. Specifically, I would like to know how the code works, how to modify it for my specific setup, and any best practices or tips for working with SPI communication.

    Thank you for your time and assistance with this matter. I look forward to hearing back from you soon.

    Regards,

    Adil

  • Hi,

    Sorry for the delay.

    Based on your questions I think you need to become more familiar with the mmWave SDK development environment.

    This information applies to the AWR1843BOOST

    If you have not done this already please download the SDK 3.6 and run the mmWave SDK demo as described in the mmWave SDK User Guide.

    Regarding PI, you will need to contact the PI support community.

    If you need any assistance with SDK please let us know

    thank you

    Cesar