Other Parts Discussed in Thread: OPT4048
I installed the software and it works fine, but I always shows a warning in the log file during start-up (see below)
I am not sure if this affects the reading of the calibration data as described in 3.8.1.1 of the manual where it states that it reads the calibration data from the EVM flash memory.
#======
#Executing .. OPT4048/OPT4048DTS_EVM/devInit.py
#Start Time 2023-02-10 13:19:30.643000
Registers View - No Capture Device defined
Registers View - Reset property was not found
#================ ERRORS:0, WARNINGS:2 ================#
#================ ERRORS:0, WARNINGS:0 ================#
#================ ERRORS:0, WARNINGS:0 ================#
#================ ERRORS:0, WARNINGS:0 ================#
#================ ERRORS:0, WARNINGS:0 ================#
Setting Device to 16 sensor mode
MONCx186a; Sending command to set oneshot settings
MONPx186a; Sending command to set oneshot settings
MONCx186a; Sending command to set oneshot settings
MONPx186a; Sending command to set oneshot settings
#================ ERRORS:0, WARNINGS:0 ================#
#Done executing .. OPT4048/OPT4048DTS_EVM/devInit.py
#End Time 2023-02-10 13:19:35.998000
#Execution Time = 5.35500001907 s
#================ ERRORS:0, WARNINGS:0 ================#