This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: How to configure the LVDS data rate?

Part Number: AWR2944
Other Parts Discussed in Thread: DCA1000EVM,

Hello experts,

I use the oscilloscopes to monitor  the LVDS data rate, and find that it is 450MHz. Then I set the hsiClkgs.hsiClk to 0xB or other values in mmwave_link_mailbox.c, but the LVDS data rate is still 450MHz, not that I'd want to be.

Also, I try to call the API of rlDeviceSetDataPathClkConfig to configure the LVDS data rate, but still ineffective, and this API return value is -12, it seems API called is not supported.

So how to configure the LVDS data rate effectively? 

Many thanks.