Hi Team,
There is no detailed description of the starting frequency, bandwidth, and slope used during calibration in the calibration document. So I have the following questions.
1. Is constant frequency calibration required during calibration?
2. How does the choice of center frequency during calibration affect PS INL?
3. Since the calibration itself also has the problem of jitter in the measurement data, does the calibration operation require N times of calibration to obtain the expectation?
4. If N operations are required, what is the value range of N?
5. Is this measurement noise Gaussian, and can we use the mean instead of the expectation?
Kind regards,
Katherine