Other Parts Discussed in Thread: PGA460, ENERGIA
Hi,
In our Application, we need to detect objects above 11 meters. I followed the same steps mentioned in the PGA460 Frequently Asked Questions (FAQ) and EVM Troubleshooting Guide() /"How can I detect an object if it is further than 11m?".But unfortunately, we are getting the wrong data on the preset 2 listen-only command (most of the time 11.24 meters). The time between the P1BL and P2LO is less than 2 ms.
I tried reducing the REC_LENGTH of preset 1 to 4 meters and preset 2 to 5 meters and enabled the test pin and object placed at 6 meters. In this setup, we are able to see the pulse reflected echo after the Preset 2 Listen-only command. But when I turned off the test pin (verified by reading the test pin register back and no test pin signal on the scope)and start reading the ultrasonic measurement data it was giving the wrong distance(initially it was giving .7 and then 11.24 meters ).
ultrasonic sensor: CUSP-TR80-15-2500-TH(range 15 M).