This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: Required the source code for binary file in .bin format.

Part Number: AWR1642BOOST

Hello,

I'm flashing the Radar Sensor using the mmwave_sdk_02_00_00_04 prebuilt binary image - xwr16xx_mmw_demo.bin which is located in C:\ti\mmwave_sdk_02_00_00_04\packages\ti\demo\xwr16xx\mmw folder.

Now I need to see its corresponding code, means from where that binary file has come. where Can I get those codes, please help me finding that, I'm new to this domain.

also, I need to see the code because I need to understand the object detection mechanism, how the objects are being detected and for some objects it's showing static dots and for some it's showing blinking dots.

please help me finding the source code file for that binary image in .bin format.

Thank you :-)