This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243BOOST: Sensing Range

Part Number: AWR1243BOOST
Other Parts Discussed in Thread: AWR1443BOOST, AWR2243, AWR1243, AWR1443

Hi,

Good Day.

Could you please provide a sensing range for the part numbers below?

AWR1243BOOST

AWR1443BOOST

Please advise. Thank you very much.

Best Regards,

Ray Vincent

  • Hi,

    AWR1243 is a front end sensor that requires a host for processing. If you are interested in the AWR1243 device we recommend using the newer generation AWR2243 device.

    Since the AWR1243 requires a host for processing, TI does not provide a demo for the AWR1243BOOST EVM. The board can only be used together with the DCA1000 capture card for raw data capture.

    The sensing range for AWR1243/2243 is 150-200m

    AWR1443 is a programmable sensor that is supported by the mmWave SDK 2.1. There is a demo available for AWR1443BOOST

    The sensing range is 20-30m

    Thank you

    Cesar