This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Internal phase changes of the two SYNCIN pins for 20GHz LO

Part Number: AWR2243

Dear TI experts,

Is chip-internal phase change (internal circuit length) of the FM_CW_SYNCIN1 [pin# B1] different from the FM_CW_SYNCIN2 [pin# D15]?

Do we have out-of-phase issue when we use the port B1 in one slave chip and D15 in another slave chip, for example?

Thank you in advance for your advice.