Hi Team,
Can you please help with the inquiry below?
the mmWave studio software is unable to read FPGA version, indeed int the following image you can see that the FPGA Version is 0.0.0.0

[23:15:56]
[23:15:56] CaptureCardConfig_EthInit Success
[23:15:56] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 0)
[23:15:56] [RadarAPI]: Sending fpga command to DCA1000
[23:16:06] [RadarAPI]:
[23:16:06] FPGA Configuration :
[23:16:06] Timeout Error! System disconnected
[23:16:06] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[23:16:06] [RadarAPI]: Sending fpga command to DCA1000
[23:16:16] [RadarAPI]:
[23:16:16] FPGA Configuration :
[23:16:16] Timeout Error! System disconnected
[23:16:16] [RadarAPI]: Sending record command to DCA1000
[23:16:26] [RadarAPI]:
[23:16:26] Configure Record :
[23:16:26] Timeout Error! System disconnected
[23:16:26] CaptureCardConfig_PacketDelay failure
[23:16:26] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti_In_Use\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", 1)
[23:16:26] [RadarAPI]: Sending start_record command to DCA1000
[23:16:26] [RadarAPI]: Status: Passed
[23:16:27] [RadarAPI]: ar1.StartFrame()
[23:16:27] [RadarAPI]: Status: Passed
[23:16:27] Frame start async event received!
[23:16:28] Frame End async event received!
[23:16:28] [RadarAPI]: Frame Ended
[23:16:32] Please wait for a few seconds for matlab post processing .....!!!!
[23:16:32] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti_In_Use\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin")
[23:16:32] [RadarAPI]: No of files Captured: 0, Total no of frames for each device : 8
[23:16:32] Error : The number of files captured is zero!
[23:16:42]
[23:16:42] ***Script completed successfully.***