This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432: Regarding EVM board materials

Part Number: IWRL6432

Hi Radar Champ

I'd like to check a few things about EVM board raw materials.

Q1.

In the following substrate information, isola FR408HR material has a dielectric constant of 3.3?
On the manufacturer's website, the representative dielectric constant value on the datasheet is 3.68.
Is the substrate dielectric constant estimated at 3.3 because the frequency of use is 60 GHz?
Or can I get the data that measured the substrate characteristics at 60GHz?

Q2.

Except for FR408 materials, the board part will only be used as a digital unit.
Can I use a regular FR4 (er=4.4-4.6) material instead of the PCB material PCL370HR material provided below?

Thanks.

Regards, 

Jack