Part Number: FDC1004
Hello We have confirmed that the first data at the start of measurement on the FDC1004 outputs the data from the previous measurement. After measuring the capacitance of the liquid in bottle 1 and detecting the liquid level, the liquid is sucked. After that, the liquid is discharged to bottle 2, but the electrostatic capacity of the liquid in bottle 2 is measured before discharging. Capacitance measurement starts from a specific height and repeats until the liquid level is detected. The problem is that the first data when measuring the capacitance in bottle 2 may output the capacitance of bottle 1. Checking the register gives the following:
012346 A0a=>0Ca A0a<=0Da80n←Bottle 1 measurement incomplete
012346 A0a=>0Ca A0a<=0Da88n←Bottle 1 measurement completed
012346 A0a=>00a A0a<=55aF5n ← Read bottle 1 data
012346 A0a=>01a A0a<=D9a00n←Read bottle 1 data
012347 A0a=>0Ca A0a<=0Da88n←Bottle 1 measurement completed
012347 A0a=>00a A0a<=67a9An ←Read bottle 1 data
012347 A0a=>01a A0a<=AAa00n←Read bottle 1 data
012347 A0a=>0Ca00a00a ← Bottle 1 measurement stop
012710 A0a=>0Ca0Da80a ← Bottle 2 measurement start
012710 A0a=>0Ca A0a<=0Da80n←Bottle 2 measurement incomplete
012711 A0a=>0Ca A0a<=0Da88n←Bottle 2 measurement completed
012711 A0a=>00a A0a<=67a9Bn ← Read bottle 2 data
012711 A0a=>01a A0a<=1Fa00n←Read bottle 2 data
012711 A0a=>0Ca00a00a ← Bottle 2 measurement stop
The capacitance of bottle 2 is about 2pF, but 12.95pF (0x679B1F) is measured. This is equivalent to bottle 1's capacitance of 12.95pF (0x679AAA). I have this problem from time to time. This problem occurs only with the first data in bottle 2. Will there be any problems if the time from the start of measurement to confirmation of completion of measurement is too short?