Other Parts Discussed in Thread: TUSS4470, MSP-EXP430F5529LP
Hello E2E Experts,
Good day.
I cannot find the "En" checkbox or "Master" checkbox anywhere in the TUSS4470 EVM GUI. Please help me to find it.
TUSS44x0 EVM for Ultrasonic Sensors User's Guide (Rev. A)
3.5.2.5.3 External Sync and Trigger
To synchronize the time-of-flight command with an external system or another TUSS44x0 EVM, use the external sync and trigger run feature. When the En checkbox is checked, the GUI/EVM becomes a sync- slave, where BOOSTXL-TUSS44x0 pin-11 monitors for a low-to-high transition. The Master checkbox enables the GUI/EVM to act as the sync-master, such that the MSP-EXP430F5529LP forces a low-to-high transition on BOOSTXL-TUSS44x0's pin-13 when the START button is clicked in the Run Options group.
Regards,
CSC