This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC6821: RPM Accuracy Issue

Part Number: AMC6821

Hi 

In our design we are using the AMC6821 Fan controller IC, we are facing issue in RPM measurements, 

Please find the attached table, in this table Expected RPM we are not getting, As per datasheet its an +/- 7% accuracy will be acceptable, But in our case we are seeing more.

PERCENTAGE

CONFIGURED
DCY-REG VALUE

READ TACH-LOW_BYTE

READ TACH-HIGH_BYTE

READ RPM 

EXPECTED RPM

25(%)

0x40

0xa9

0x0a

2198

3275

34(%)

0x57

0xc1

0x06

3470

4454

43(%)

0x6E

0x17

0x05

4604

5633

52(%)

0x85

0xe5

0x03

6018

6812

61(%)

0x9B

0x3d

0x03

7237

7991

70(%)

0xB2

0xc5

0x02

8429

9170

79(%)

0xCA

0x76

0x02

9523

10349

88(%)

0xE1

0x3d

0x02

10471

11528

97(%)

0xF8

0xda

0x01

12658

12707

100(%)

0xFF

0xd4

0x01

12820

13100