This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: External clock capacitive load matching

Part Number: IWR6843AOPEVM
Other Parts Discussed in Thread: IWR6843AOP

Hi,

As per the IWR6843AOPEVM Rev F. schematic, calculated CL value of the  external clock source is 2.35pF, however, according to the 8.10.4.1 section of the IWR6843AOP datasheet this value should match the CL of the crystal (KYOCERA AVX CX2016DB40000D0FLJCC) which is 8pF.

Pleas let me know whether this is within the tolerance of IWR6843AOPEVM or an error in the IWR6843AOPEVM Rev F. schematic.

Thanks