Hi forum,
While running the mRR_Viz_1_4 GUI of lab0011_mrr_beamsteering from the file location "mmwave_automotive_toolbox_3_6_0\labs\lab0011_mrr_beamsteering\gui\MRRvisualization", I encountered with below error log:
Case-1: My PC operating system is 64-bit. I have installed MATLAB Runtime v8.5.1 64-bit, still I'm facing the same issue while opening the GUI.
Case-2: Secondly I tried installing MATLAB Runtime v8.5.1 32-bit, the GUI has opened successfully. But the GUI hangs after sometime.
Attached below the screenshot of GUI after hanged.
Could anyone please help me to resolve this issue.
Thanks in advance
Pragathi