Dear TI,
I have a question about the Radar Toolbox for Medium Range Radar.
I was wondering if you could help me pinpoint in the MRR_GUI tool, a section of code we could manipulate/ derive to program our Raspberry Pi.
That section of code should be able to determine distance based on information gained from AWR1843, then based on data gained over time, should be able to communicate with Raspberry Pi by turning on red or green LEDs, for instance, if the distance is too close between the car and the radar, the LED is red. And if it is at a suitable distance, the LED remains green.
Any help suggesting parts of code in MRR GUI that could help us gain the same result but used to communicate with raspberry Pi and LEDs.
It is greatly appreciated.
Thanks.