Hai all,
I am currently working on inductive sensors for longer sensing range and I came across LDC1612/1614 as a solution for the same.
But, while going through the datasheet I have a few queries:
1) what is the maximum sensing range possible w.r.t the sensor diameter. For ex., if the sensor diameter is 12mm, then what is the maximum sensing range achievable with LDC 1612 or LDC 1614.
2) whether the sensing distance measured is lateral measurement or axial measurement of the target material.
Regards,
Deepthi S. Nair.