This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: The ghost point in message

Part Number: AWR1642

Hi,

We design a board and use the ro3003g2 and find ghost point (radom speed 1x 3x 5x...) at some degrees. (AWR1642, labs SRR )

The ghost points at -30 ~  +30, when we make it in the 3 meters chamber.

And we put the hand in front of it, it also appear the ghost point.

I try to use TX1 and TX2 whit RX1 ~ RX4 setting

And I find just only use two RX is no problem.  RX_CHANNEL_1_2_ENABLE RX_CHANNEL_1_3_ENABLE RX_CHANNEL_1_4_ENABLE RX_CHANNEL_3_4_ENABLE...

May you give some advice to me?

Thanks