This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: AWR1843 Boost hung up for a config file

Part Number: AWR1843BOOST

We are flashing a config which shows okay on sensing estiamtor from TI: (link of snip https://drive.google.com/file/d/1mJBoHHvXBQhnw-COcwWhImLOiXWzCnqH/view?usp=share_link)

However the sensor hangs on demovisualizer after a few seconds with the following error showing up: https://drive.google.com/file/d/1aVLWeD8px13OoPczn7KFCw1-NBk4LYMQ/view?usp=share_link

The config file using on AWR 1843 boost is as:

https://drive.google.com/file/d/1EBre3Xim3eM76UemUeUMqV_iAwBIZ4M3/view?usp=sharing

Please guide me why this may be the case, and how to go about the problem in the config file

  • Hi Mihir,

    Can you please upload the attachments as text or images directly in your query? I will not be able to access the drive links you have shared.

    Regards,

    Kaushik

  • Config file: 

    % ***************************************************************
    % Created for SDK ver:03.06
    % Created using Visualizer ver:3.6.0.0
    % Frequency:76
    % Platform:xWR18xx
    % Scene Classifier:best_range_res
    % Azimuth Resolution(deg):15
    % Range Resolution(m):0.288
    % Maximum unambiguous Range(m):20.07
    % Maximum Radial Velocity(m/s):6.52
    % Radial velocity resolution(m/s):0.82
    % Frame Duration(msec):100
    % RF calibration data:None
    % ***************************************************************
    sensorStop
    flushCfg
    dfeDataOutputMode 1
    channelCfg 15 5 0
    adcCfg 2 1
    adcbufCfg -1 0 1 1 1
    profileCfg 0 76 7 8 95 0 0 12 1 225 3000 0 0 30
    chirpCfg 0 0 0 0 0 0 0 1
    chirpCfg 1 1 0 0 0 0 0 4
    frameCfg 0 1 80 0 50 1 0
    lowPower 0 0
    guiMonitor -1 1 1 1 0 0 1
    cfarCfg -1 0 2 8 4 3 0 15 1
    cfarCfg -1 1 0 4 2 3 1 15 1
    multiObjBeamForming -1 1 0.5
    clutterRemoval -1 0
    calibDcRangeSig -1 0 -5 8 256
    extendedMaxVelocity -1 0
    lvdsStreamCfg -1 0 0 0
    compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
    measureRangeBiasAndRxChanPhase 0 1.5 0.2
    CQRxSatMonitor 0 3 4 25 0
    CQSigImgMonitor 0 39 4
    analogMonitor 0 0
    aoaFovCfg -1 -90 90 -90 90
    cfarFovCfg -1 0 0 18.45
    cfarFovCfg -1 1 -6.52 6.52
    calibData 0 0 0
    sensorStart

    sensing estimator screenshot

    Demovisualizer hung up:

  • Hi Mihir,

    I am not able to see any error logs in any of the images shared. Can you please point me to it?

    Regards,

    Kaushik