This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243BOOST: CSI frame end packets

Part Number: AWR2243BOOST
Other Parts Discussed in Thread: AWR2243

I'm trying to read the raw ADC data from the AWR2243 radar chip using a Raspberry Pi via CSI2. Upon inspecting the CSI transaction I've noticed that the radar does not send the end-of-frame packet and the raspberry, therefore, can't receive the frames properly. Maybe I'm missing something in the settings so that it happens much later than the transaction? I tried to play with the frame parameters in the mmwave studio, ie setting the frame periodicity such that it should have one CSI transaction, with the number of frames and the number of loops settings, but no luck. Could you please clarify what are the conditions to get EOF packet?