This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
I'm using mmWaveStudio 3G as recommended for IWRL6432BOOST along with DCA1000 for data capture.
I have flashed the board with the presence_and_motion_detection.appimage file (here: "C:\ti\MMWAVE_L_SDK_05_01_00_04\examples\mmw_demo\motion_and_presence_detection\prebuilt_binaries\motion_and_presence_detection_demo.release.appimage")
After which I changed board to the functional mode.
Now, I am using the mmWaveStudio to interface with the board and configure the parameters in the lua script mentioned in the path (here: "C:\ti\mmwave_studio_04_01_00_01\mmWaveStudio\Scripts\MatlabExamples\LUA_examples\chirp_60G_6m.lua")
While starting the mmWaveStudio, we run the common_device_setup.lua from ("C:\ti\mmwave_studio_04_01_00_01\mmWaveStudio\Scripts\MatlabExamples\LUA_examples\common_device_setup.lua")
After which I run the config lua file that will trigger the data capture.
Is the process correct? Please correct if the process is wrong or need any adjustments.
Thanks in advance.
Hello,
Please refer to the DCA1000 User's Guide, in which detailed instruction is provided for the usage of the DCA1000 with our various devices, including the IWRL6432.
Regards,
Luke