Other Parts Discussed in Thread: IWRL6432
Hi Expert,
I'm using mmWaveStudio 3G as recommended for IWRL6432BOOST along with DCA1000 for data capture.
I have flashed the board with the presence_and_motion_detection.appimage file (here: "C:\ti\MMWAVE_L_SDK_05_01_00_04\examples\mmw_demo\motion_and_presence_detection\prebuilt_binaries\motion_and_presence_detection_demo.release.appimage")
After which I changed board to the functional mode.
Now, I am using the mmWaveStudio to interface with the board and configure the parameters in the lua script mentioned in the path (here: "C:\ti\mmwave_studio_04_01_00_01\mmWaveStudio\Scripts\MatlabExamples\LUA_examples\chirp_60G_6m.lua")
While starting the mmWaveStudio, we run the common_device_setup.lua from ("C:\ti\mmwave_studio_04_01_00_01\mmWaveStudio\Scripts\MatlabExamples\LUA_examples\common_device_setup.lua")
After which I run the config lua file that will trigger the data capture.
Is the process correct? Please correct if the process is wrong or need any adjustments.
Thanks in advance.