This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2214: FDC2214

Part Number: FDC2214


Hi. 

I am using fdc2214 chip to measure capacitance. I have designed a circuit that includes buffer opamp configuration for active shielding. My opamp is mcp654 which has 50MHz GBW and 30V/us slew rate.

C = 33pF and L = 22uH are the components that are used for the LC tank circuit. My resonance frequency is 3.27MHz. When i check the frequency of the resonance circuit alone i see 3.27MHz. Then i used two channels of the oscilloscope to see the active shield and the LC resonance signal at the same time. Again i see 3.27MHz as the figure given below.

 

But when i try to observe buffer output (active shield) alone i see a signal at 4.39 MHz as given below. I don't get it.

They should always be the same. What do you think is the problem? How can i solve it?

Thanks in advance.

  • How do the waveforms compare between the op amp input and the op amp output?

    If they look different, one easy thing to try would be to add a little series resistance between your op amp output and your shield.
    The shield is usually a large capacitance, and some op amps have a hard time driving highly reactive loads.
    If that is the root cause you may have to experiment with the resistance value.

    Regards,
    John

  • There is no shield (capacitor plate) at the moment. I just used the LC resonance signal and fed it to the input of the buffer. But the frequency of the input and output is different. When i check them both at the same time they have the same frequency but when i measure only the shield signal it is different than the input. I don't get it. Hope you can help.

  • How are you probing the resonance signal and the input to the buffer?

    John