Hello,
When two AWR1642s are driven separately in parallel, they are influenced by each other and sometimes not.
It was experimentally confirmed that there was no significant effect on each other when placed at a close distance.
They were placed facing each other to be most affected, and when operated several times, only a few times were affected and the rest were not affected.
So, I have a question, when operating multiple radars at the same time, each radar receives its own Tx signal.
Recently, I heard that signal processing is being proposed to accept only signals sent by the radar itself.
I don't know much about the field, like.. distinguishing signals through Tx modulation
Has this been applied to TI radars??
If applied, can I turn it off?
Thank you.