1)In the demovisualizer, plots show relative power vs range as below:
a)
b)
I ran a set of tests while keeping the same object in front of it, to evaluate the configs. For the same object, does a higher relative power mean a greater probability of detecting similar objects at longer distances, when compared to configs showing up the same object with lower relative power? For eg: in the graph above, configs corresponding to (a) has higher probability of detecting objects at longer distances when compared to (b)
2) I used the following configuration, which seems to be out of memory bounds, however still runs with the radar. Am I doing something wrong here?
The memory consumption comes out to be 480*3*32*0.031 kb = 1400 kb instead of maximum limit of 1024 kb?
3) Is it possible to do beam steering using the default xwr18xx_mmw_demo.bin file simply by sending profile congifs, with txphase shifter set to desired value?
I am sending the config below,which runs without any issue. Does it mean that beam steering is enabled. Is there a place where I can get the config file for beam steering in the format mentioned below, instead of a .c/.h file?
sensorStop
flushCfg
dfeDataOutputMode 3
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 76 7 6.4 40 0 8174592 18 1 320 10000 0 0 30
profileCfg 1 76 7 6.4 40 0 13953024 18 1 320 10000 0 0 30
profileCfg 2 76 7 6.4 40 0 2889728 18 1 320 10000 0 0 30
profileCfg 3 76 7 6.4 40 0 8668160 18 1 320 10000 0 0 30
chirpCfg 0 0 0 0 0 0 0 7
chirpCfg 1 1 1 0 0 0 0 7
chirpCfg 2 2 2 0 0 0 0 7
chirpCfg 3 3 3 0 0 0 0 7
advFrameCfg 4 0 0 1 0
subFrameCfg 0 0 0 1 32 80 0 1 1 80
subFrameCfg 1 0 1 1 32 80 0 1 1 80
subFrameCfg 2 0 2 1 32 80 0 1 1 80
subFrameCfg 3 0 3 1 32 80 0 1 1 160
lowPower 0 0
guiMonitor -1 1 1 0 0 0 1
cfarCfg -1 0 2 8 4 3 0 8 0
cfarCfg -1 1 0 4 2 3 1 18 0
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
lvdsStreamCfg -1 0 0 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 5 121 0
CQSigImgMonitor 0 127 4
analogMonitor 0 0
aoaFovCfg -1 -30 30 -90 90
cfarFovCfg -1 0 3 20
cfarFovCfg -1 1 -1 1.00
calibData 0 0 0
sensorStart