Hi all
I want to increase the chirp start frequency of every chirp in a frame by a fix step.
for example. the start frequency of first chirp is 77GHz, the second is 77G+1MHz, the third is 77G+2MHz and the 128 chirp is 77G+128MHz
So i use the advance chirp function to do this just as below
But if i call the" MMWL_advChirpConfig " and only config the
CHIRP_FREQ_START_VAR |
(Chirp Param Idx = 1)
Then the chip will report errors ,the error code is 311
This error means
So if i want to use "Advance chirp config" function,do i need config all the Chirp Param Idxs from 0 to 9?
Thanks