Other Parts Discussed in Thread: AWR2944, UNIFLASH, DCA1000EVM,
Hi team,
Here's an issue from the customer may need your help:
Issue: Raw data cannot be captured using AWR244EVM with DCA1000
The customer had referenced this thread and done the following:
1) For two boards: XDS_USB and FTDI connect to PC via data cable, connect network cable and configure IP, and two boards connect 60-row cable.
2) The awr2944 was burned in 101 mode using uniflash. The burning files are as follows:
E:\ti\mmwave_mcuplus_sdk_04_03_00_01\mmwave_mcuplus_sdk_04_03_00_01\tools\awr294x\sbl_qspi.release.tiimage
E:\ti\mmwave_mcuplus_sdk_04_03_00_01\mmwave_mcuplus_sdk_04_03_00_01\ti\demo\awr294x\mmw\awr2944_mmw_demoTDM
3) Connect awr2944 in 100 mode with mmWave_Demo_Visualizer/ver/4.3.0/, it can connect successfully and it can be found there's no problem through the test.
4) Power the board back on and connect mmWave_Demo_Visualizer and DCA1000. Execute the following command from the command prompt C:\ti\mmWave_studio_03_00_00_14\mmWaveStudio\PostProc directory (the corresponding AWR294x_Capture has been copied to this directory):
DCA1000EVM_CLI_Control.exe fpga AWR294x_Capture.json
success
DCA1000EVM_CLI_Control.exe start_record AWR294x_Capture.json
success
5) Returns mmWave_Demo_Visualizer/ver/4.3.0 and load the following directory cfg file in plot:
E:\ti\mmWave_mcuplus_SDK_04_03_00_01\mmWave_mcuplus_SDK_04_03_00_01\ti\demo\awr29 4x\mmw\profiles\tdm_awr2944\profile_LVDS
The case here is once the above process was done, you will still see the various graphs in Visualizer. However, after clicking sensor stop, the bin file is not generated in the corresponding location, and the data_Tran_PRG on the DCA1000 stays on solid and does not blink. The generated awr294x__HDR_LogFile shows that no data was captured (with the same capture start time and capture end time).

So how to capture the raw ADC data?
Could you please help check this case? Thanks.
Best Regards,
Cherry