This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA970: PGA970

Part Number: PGA970

Dear Ti Engineer, 

I have got a PGA970evm with me and trying to connect a half-bridge sensor to it, I am using a circuit diagram suggested by  Ti engineer. According to the data sheet S1N, S1P, S2N, and S2P pins can only tolerate voltages up to 3.45V and I am powering the PGA970EVM board by 12V which caused the chip to blow. Reducing the supply voltage to under 6V will distort the signals at  P1 and P2 (peaks will clip).  Is there a way to power the chip with lower voltages? Am I missing a step? Or do I need to attenuate the output signal form my Half-bridge sensor?

 

Thank you in advance

Nasser Ashouri