Hello Team,
Posting on behalf of my customer:
We have bought an FDC1004EVM and try to get it to work with our self-made 'flex-PCB' (along the design rules of TIDU736A, regarding references, shields and symmetry) with the Out of Phase technique.
When we follow Section 5.2 of the design guide to set the right configuration for CHA and CHB, we end up with seturated values, see attached screenshot. CIN4 is floating and we are trying to measure the water level in a plastic bottle.
We saw in the SNOA925 document that the ground is connected to the shields, but in the design guide, this is not the case. Which one to follow?
We hope that the Out of Phase technique fixes some of the issues we have now, such as a higher capacitance for the RE than for RL. Also, when we shake a bottle of water with the flex-PCB on it, the final values are higher than the starting ones, although the water level has not changed.
Could this be because of the Out of Phase technique that is not working, or is something else wrong?
We have tried to set an offset to overcome the saturated value. However, then the capacitance values still do not change in time.
Regards,
Renan