This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6443: 6-bit linear phase modulation presence

Part Number: IWR6443
Other Parts Discussed in Thread: IWR6843,

Team,

Can you confirm that the 6-bit linear phase modulation which is mentionned in the IWR6443 datasheet (swrs219e p59) is also available in the IWR6443 since the section 9.3.1.2 mentions explicitly IWR6843 instead of both 6843 and 6443 (while at the same time the difference is not listed in table 6-1).

Thanks!

MCV