This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: Question about "HWA Advanced Statistics – 2-Dimensional Maxima" in ES2.0

Part Number: AWR2944


Hi

      In AWR2944 ES2.0, we found that the Advanced Statistics about 2-Dimensional Maxima has different performance compare with ES1.0

      We use a single hwa parameter to config 2-Dimensional Maxima and get 2D maxima, but in ES2.0, this function can provide current index, but can't provide current value, the range of variation from 5 to 30.

      We use another max engine: fft out mode: HWA_FFT_MODE_OUTPUT_MAX_STATS, it has same result: this engine can provide current index, but can't provide current value

      If we change to ES1.0, both value and index are correct.

      Is there any updates can effect the Max engine value result?

Thanks

Patrick