Hi all
When I use the function of advance chirp, i am confused about the LUT address
for example
1、When i config the 8 profiles, it means the address from 0x0 to 0x7 is profile 0 to 7 ,the unit is BYTE
2、Then i config 8 start frequency, because of the lutChirpParamSize is 1, so one start frequency need 2 Bytes
So it means the address from 0x8 to 0x17 is start frequency
So Do my understand is correct?
if my understand is correct, i want to config 2 subframe. how can i write the parameters of the second subframe?
Thanks