Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843AOP: Custom board without 60 pin Connector

Part Number: AWR6843AOP

Hi,

I have developed a custom board with AWR6843AOP, but due to small size of the module I had not space for 60 pin connector.

I have the UART connection available and I get connection with mmWave Demo Visualizer.

Can I connect the device with mmWave Studio? Device is not detected in the Connection Tab.

I would like to start with certification FCC/RED and from app note, I see a Lua scipt ir requested for Stability frequency Test.

I found Lua script in the certificatoin package, but how can I run the Lua script, without mmWave Studio?

Thanks a lot,