Other Parts Discussed in Thread: IWR6843
IWR6843ISK did not explain the operating temperature.
Am I correct in understanding that it is the same as the IC operating range temperature?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
IWR6843ISK did not explain the operating temperature.
Am I correct in understanding that it is the same as the IC operating range temperature?
Hi,
The IWR6843ISK has been tested in the 60-64GHz band across the temperature range of -20°C to 60°C. The device is intended for use within the aforementioned limits.
The IWR6843 EVM operates at a maximum duty cycle of 50%, running at a higher duty cycle increases the risk of damaging the EVM by exceeding the maximum operating junction temperature (Tj ) of 105°C.
Regards
Ankit