Good morning Technical
I have a hydraulic motor mounted on a horizontal plate with an output shaft that has a bevel gear. The other end of the shaft protrudes from the non-drive end of the hydraulic motor enough to get a sensor to count or measure. The bevel gear meshes into another gear at right angles, with a larger diameter bevel gear and this shaft rotates to open and close a valve. The ratio is never 1.1 and can vary on every application. I would like to be able to display the position of the valve on a digital display showing the % open from 0-100. I was looking at a pulse (inductive sensor) to analog converter to enable the 4-20mA to be scaled, however when the valve shaft travels in the opposite direction the converter wouldn't know. I wondered if I could insert a magnet into the shaft and when the shaft went clockwise, a sensor would detect a north pole and when it went anticlockwise, a south pole. I am looking for a solution that requires 12 or 24VDc supply. I require a solution for ten systems, but this will increase.