Other Parts Discussed in Thread: MMWAVEICBOOST,
Hi,
Until now I’m developing the target software with an IWR6843AOP EVM plus a MMWAVEICBOOST carrier board. The use of the RS232 channel to configure the application (CLI interface) plus the additional RS232 Tx data link seems to be the way we go for the application.
For further development I’d like to use our own target hardware and want to replace the MMWAVEICBOOST carrier board with an XDS110 Debug Probe. As a first step of the replacement of the carrier board with the XDS110 I’ve connected the XDS110 debug interface with the 14pin JTAG connector of the MMWAVEICBOOST carrier board. I’ve also connected the Rx and Tx line of the XDS110 AUX function interface with the J5 connector of the MMWAVEICBOOST carrier board. The DIP switches S1.1 to S1.11 of the carrier board are set as listed in table 2.1 column “Position for 40-Pin LP/BP” of the user’s guide “60GHz mmWave Sensor EVMs”. S1.12 is set to position OFF.
The question I have is how to connect the data link that is available on pin 9 of J6 on the carrier board with the XDS110? I’ve tried to use the expansion connector on the XDS110 but I do not receive any data on the viewer software as I do when using the MMWAVEICBOOST carrier board as debugger.
Thanks for your advice