Other Parts Discussed in Thread: MMWAVEICBOOST,
I'm using IWR6843ISK-ODS with the MMWAVEICBOOST. I need to find the output power of the on-board GPIOs. How much is the current carrying capacity of each pin?
Regards,
Purvi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm using IWR6843ISK-ODS with the MMWAVEICBOOST. I need to find the output power of the on-board GPIOs. How much is the current carrying capacity of each pin?
Regards,
Purvi
Hi Purvi,
I am looking into your question and will get back to you soon.
Regards
Ankit
Hi Purvi,
All the I/Os operate on VIOIN power supply which can operated through 3.3 or 1.8V. The GPIO pins consume negligible power when not in use. The maximum sink/source current on the GPIO is 6 mA.