This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843AOPEVM: CC2640R2F Integration

Part Number: AWR1843AOPEVM
Other Parts Discussed in Thread: CC2640R2F, , CC2642R, CC2652R

Dear TI Team,

I have a question that is similar to one asked on this forum post: https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1203629/awr1843aopevm-awr1843aopevm/4541057?tisearch=e2e-quicksearch&keymatch=AWR1843AOPEVM%20bluetooth#4541057. However, I am having difficulty understanding the response provided by the TI expert.

I am using the AWR1843AOPEVM, which includes a CC2640R2F Bluetooth module. Based on the schematics of the AWR1843AOPEVM, it appears that the UART and logger output of the AOP device are connected to the Bluetooth chip (as well as to the UART-USB converter chip).

Currently, I am able to interact with the EVM via USB to use the cloud-based visualizer. However, I would prefer to communicate with the AOP through the Bluetooth interface. When I power up the EVM, I see a Bluetooth device named "Simple Peripheral," but I have not been able to find any information about using Bluetooth with the EVM.

Do I need to flash the on-board CC2640R2F with specific code to enable it to work with the EVM? Additionally, do I need any additional hardware to perform the flashing?

Please advise us on the next steps.

Best regards,

Gagandip Singh Dadhwal