Other Parts Discussed in Thread: TMP1075, TMP275, TMP112
Hi team,
Several questions on I2C setting for the device.
1. During the POR event, does I2C bus go idle as well? (No need to apply 9 clock or other reset through I2C?)
2. Datasheet says that the SDA of the I2C bus may be set to "L" and stopped while reading the temperature.
At this time, the stop can be reset by applying 9 clocks (until SDA becomes "H").
Also, Note 17 of Electrical Characteristics states that if SDA or SCL remains "L" for the timeout period or longer, the device itself resets (SDA and SCL to "H").
Does the user need to apply the clock because SDA can stop at 'L'? Or is it not necessary to apply a clock(logic) such as because the device can reset itself due to timeout?
Also, do we have a newer device suggestion?
Regards