This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: Making connections wireless

Part Number: IWR6843AOPEVM


Hello,

I am using IWR6843AOPEVM Rev G and DCA1000 together to collect raw data. The setup has 4 connections; 3 of them to the DCA1000 and 1 to IWR6843AOPEVM. Power, ethernet, and RADAR FTDI micro USB to DCA1000, and Emulator USB port for user UART and Data COM ports to IWR6843AOPEVM.

I was wondering if is there any way to make these connections wireless (except the power of course), like a wifi or Bluetooth interface?

Thank you.

Best,

Yahea

  • Hello Yahea,

    Due to the sheer quantity and speeds required to do raw data transfer, it is for that reason Ethernet is required. WiFi may be possible, but we have no current experience nor have any plans to support this so it would have to be all custom made.

    Best Regards,

    Pedrhom