This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: NERR LED is constantly on. Board is drawing more current than it used to.

Part Number: IWR1843BOOST
Other Parts Discussed in Thread: DCA1000EVM

Hi, I've been playing around with the IWR1843BOOST as part of the DAC1000 eval kit. I noticed that the NERR LED (DS1) is glowing and also the whole kit seems to be drawing more current than it was earlier. Not sure if the radar board or the DCA1000 is drawing the excess current. Combined, they were drawing ~1A previously, now they're drawing almost 2A. The only documentation I could find just says "HW Error". Is there a list of specific errors I can look at to help troubleshoot?