This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-DSP-EVM: Facing issues with MMW CAS DSP evaluation board (PROC055 B 001). Used PROC055E6 previously with no issues.

Part Number: MMWCAS-DSP-EVM
Other Parts Discussed in Thread: MMWCAS-RF-EVM

Facing issues with MMW CAS DSP evaluation board (PROC055 B 001). Used PROC055E6 previously with no issues.

Unable to save data after capturing on B001 board using Linux demo from PROCESSOR SDK VISION (Cascade capture & data collection). Same settings, boot switch, and config applied as with PROC055E6.

Tested the B001 board with MMWaveStudio capture demo - it worked fine. Issue persists with both modified and original Linux demo versions (Both worked well on E6 board).

Wondering if B001 doesn't support VISION SDK Linux demo like E6 board. Please help verify.

Additional info:

  • Linux demo project has multiple demos.
  • Tested "Test SSD Write" - successfully stored files on SSD, so PCIe SSD is not the issue.

Need guidance to fix this problem. Thanks in advance for your help!