Hi Team,
Good day.
I have a question about the echo data dump that is received from the UARX. the export data from the GUI have 128 values from the measurement. But when reading from UART while using the GUI-program there is only around 110.
Here is an example for reference:
Data from text export:
250 251 255 255 244 123 23 170 219 146 36 28 57 49 18 78 83 38 40 30 35 12 11 20 44 41 24 15 19 14 21 20 30 30 10 6 5 8 45 45 40 56 38 184 215 91 255 255 202 234 115 167 255 255 243 94 32 203 203 50 19 16 16 20 20 12 9 16 18 17 18 16 15 11 9 8 10 117 150 83 36 35 36 42 35 38 50 39 23 41 34 48 44 10 12 12 16 18 20 18 11 19 20 16 12 12 13 15 15 8 8 5 10 10 4 9 8 5 11 11 8 5 13 13 5 6 7 10
Data from reading UART:
250 251 255 255 244 123 23 170 219 146 36 28 57 49 18 78 83 38 40 30 35 12 11 20 44 41 24 15 19 14 21 20 30 30 10 6 5 8 45 45 40 56 38 184 215 91 255 255 202 234 115 167 255 255 243 94 32 203 203 50 19 16 16 20 20 12 9 16 18 17 18 16 15 11 9 8 10 117 150 83 36 35 36 42 35 38 50 39 23 41 34 48 44 10 12 12 16 18 20 18 11 19 20 16 12 12 8 10 11 13 7
Should these be completely equal?
Would you kindly check?
Thanks in advance.
Regards,
Marvin