This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: library re-build

Part Number: IWR6843

Hi,

I'm trying to re-build the cli library and get the following error:

C:\ti\mmwave_sdk_03_05_00_04\packages\ti\utils\cli>C:\ti\ccs1220\ccs\utils\bin\gmake all
SHMEM_ALLOC is set to 0x00000006
if [ ! -d "lib" ]; then mkdir lib; fi
! était inattendu.
clilib.mak:43: recipe for target 'cliLib' failed
gmake: *** [cliLib] Error 255

The .d and .ore4f files got generated fine. The corresponding . aer4f file got cleared. Before the "gmake all" command I had issued the "gmake clear" command. 

Thanks for your help

Achim