Hi Expert,
I am posting this on behalf of the customer. I have shared the full details of the inquiry below.
I have an AWR1642Boost board that I can't connect to it via the TI demo visualizer.
The tests I've done were under the following conditions:
Demo visualizer version: 3.6
SDK version: both 3.5 and 3.6
SOP Mode: 1 (Functional)
Application Port: COM3
Auxilary Data Port: COM4
Firmware: xwr16xx_radarss.bin provided in mmWave Studio firmware folder.
The board is detached from DCA1000.
I also tried SOP0 and SOP2 modes but each time only the Application port can connect to the device, and the Data port is unable to be connected to.
Could you please help me with this?
Thank you in advance for your support.
Best regards,
Jonathan