This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843AOP: HCC hard-coded start exception

Part Number: AWR1843AOP

Hi team,

The customer is trying to port HCC hard coded startup (HCC_CLI.c) from RadarToolBox to 1843aop's project. The previous hard-coded startup method was to manually call the MmwDemo_CLIxxxx function directly in sequence, and it was able to start the RF normally. After changing to the HCC, all the commands are done from the console log, and the mmWave_start and config are reported without error, and the RF current goes up. But no RF results are returned.

The hard code starts the same instructions and the console prints the same, except for the RF behavior. What might be the possible cause of the issue? Thanks.

Best Regards,

Cherry

  • Hi Cherry,

    We will need more information for this use case.

    1) Please provide the code snippet of HCC_CLI.c with the modifications you are using.

    2) Which example project for 1843 AOP are you using form the resource explorer.

    3) Please provide a snap shot of the command prompt in the current scenario when you run the modified example.

    Thanks,

    Pradipta.