This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: HSM

Part Number: AWR2944


Hi team,

The customer currently has the demo board for AWR2944 HSM version, power up the print information and then resolve it through 4834.uart_boot_socid.py script as follows:

SoC ID HSM Sec ROM Info:
---------------------------
Prime : 0x1
Key Rev : 0x2
Key Count : 0x1
SWRV SBL : 0x0

However, according to doc, the value of Key Rev cannot be greater than the value of Key Count, right?

Also, the demo board has written the key to become an SE device. How to flash the SBL into the serial port? Is it required to provide a signed UART_awr294x_EVM_flash_programr_release.tiimage file to flash? Coyuld you help share key files for SE device?  Thanks.

Best Regards,

Cherry