This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Issue with data rate

Genius 17695 points
Part Number: IWR6843

Hi Experts,

Seeking your assistance on this query from Cx:

I have an issue with the radar. When I set the sampling rate to very high, my computer won't receive the correct data through the internet.

I wonder if it is the problem with the radar. The radar type is xwr6843.

Also, when I set the sampling rate being 2000ksps and frame periodicity being 2ms, the data rate I collect from radar is 24 MBps which is correct. But when I increase the sampling rate to be 4000ksps, the data rate I coolect becomes 38 MBps, which is surely incorrect and experiencing data loss. I wonder if it is the issue with the radar's network interface.

Thank you.

Regards,
Archie A.