This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843AOP: AWR6843AOP : How do I create a 2D scatter plot instead of a 3D scatter plot in mmWave demo visualizer 3.6?

Part Number: AWR6843AOP

In the process of radar calibration, I hope to get the information of distance and angle.
Compared with 3D scatter plot, 2D scatter plot is more intuitive.
Would like to ask how to adjust to 2D scatter plot in version 3.6?




  • Hi,

    You can click and hold on that 3D plot to look at a top-down view so you only see 2D points like so:

    Additionally, I would recommend taking a look at our Industrial Visualizer in the Radar Toolbox. The plotting is much better on that visualizer and you can click and drag around in the same manner to switch from 3D to 2D views.

    Regards,

    Tim

  • May I ask why 2D scatter plot can be displayed on 6843, but not on AWR3843AOP?
    There are a lot of software in the Tool Box you are referring to. Which software can help me get information similar to 2D scatter plot?

  • Hi,

    The 2D scatter plot should work for all 6843 devices, where are you seeing that it's only the AOP device?

    I would highly recommend using the Industrial Visualizer as mentioned above located at: <RADAR_TOOLBOX_INSTALL_DIR>\tools\visualizers\Industrial_Visualizer. You can show 2D or 3D views on that visualizer very easily.

    Regards,

    Tim